AXIS#.VL.ARPF1 TO AXIS#.VL.ARPF4

Description

AXIS#.VL.ARPF1 sets the natural frequency of the pole (denominator) of AR filter 1. This value is FP in the approximate transfer function of the filter:

ARx(s) = [s²/(2πFZ)² +s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]

 

The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:

AR1, AR2, AR3, and AR4 are used in velocity and position mode, but are disabled in torque mode.

Discrete time transfer function (applies to all AR filters)

The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:

s ≈ (1-z-1)/t, where t = 62.5 µs

The poles are prewarped to FP and the zeros are prewarped to FZ.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

5 to 5,000 Hz

Default Value

AXIS#.VL.ARPF1: 675 Hz

VLARPF2 to VLARPF4: 500 Hz

Data Type

Float
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
AXIS1.VL.ARPF1

5011h

10h

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARPF2

5011h

11h

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARPF3

5011h

12h

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARPF4

5011h

13h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARPF1

5111h

10h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARPF2

5111h

11h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARPF3

5111h

12h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARPF4

5111h

13h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.ARPF1

6000

1770

Signed32

Read/Write

-

AXIS2.VL.ARPF1

71536

1177

Signed32

Read/Write

-

AXIS1.VL.ARPF2

6001

1771

Signed32

Read/Write

-

AXIS2.VL.ARPF2

71537

1177

Signed32

Read/Write

-

AXIS1.VL.ARPF3

6002

1772

Signed32

Read/Write

-

AXIS2.VL.ARPF3

71538

1177

Signed32

Read/Write

-

AXIS1.VL.ARPF4

6003

1773

Signed32

Read/Write

-

AXIS2.VL.ARPF4

71539

1177

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.ARPF1

6000

Float

Read/Write

-

AXIS#.VL.ARPF2

6001

Float

Read/Write

-

AXIS#.VL.ARPF3

6002

Float

Read/Write

-

AXIS#.VL.ARPF4

6003

Float

Read/Write

-